Other Parts Discussed in Thread: LM5021
Hi, I am currently designing and using the UCC28780 circuit.
I use EXCEL design Calculator of the UCC28780.
For the following specifications, how should the condition be entered?
Condition : 85Vrms~276Vrms / 50Hz 、 30W/32V output (peak power : 200W、Assuming audio amp, load range is wide)
Could you tell me how to fill in Excel sheet C16 ~ C24?
Please tell us about the maximum duty.
Should the designer design the worst to be less than 0.5, just like a typical flyback?
(If the calculation result exceeds 0.5, should the specifications be reviewed?)
Could you give me an example of the transformer parameter entry on the calculation sheet?
If the input condition is set to the world wide specification (85Vrms ~ 276Vrms), it is troublesome because D-max exceeds 0.5.