The datasheet is not clear for the minimum Vin for a Vout of 3.3V for the TPS62802.
The datasheet says the minimum Vin is 1.8V, but since this is a Buck Supply that is not possible for this part.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The datasheet is not clear for the minimum Vin for a Vout of 3.3V for the TPS62802.
The datasheet says the minimum Vin is 1.8V, but since this is a Buck Supply that is not possible for this part.
Hi,
The datasheet describes the Vin for TPS6280x family in general. Hence, the input Voltage Range is from 1.8 V to 5.5 V.
Of course, it is required to have higher Vin for a buck converter. To get an output of 3.3V, it is required to set a higher Vin taking into consideration that we do not have 100% efficiency. It is not possible to specify any minimum Vin for a particular output voltage. This depends on the application mainly, the load conditions and the losses in the circuit.
I hope I could answer your question.
Regards,
Febin