The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62110-HT: synchronous buck converter

Part Number: TPS62110-HT
Other Parts Discussed in Thread: TPS62110

hi everyone,

I'm running a Trial version of PSpice. I downloaded PSpice model and a project example TPS62110 PSpice Model (Rev. B). the simulation is for a downhole application (high temperature) knowing that the TPS62110-HT buck converter withstand to 175°C i runned the simulation for 150°C and i had this error "INTERNAL ERROR -- Overflow in device X_U1.D_U2_D1, Convert"

i used transient model for the TPS62110 and i runned the simulation in Time domaine (transient),  i used autoconvergence and put DMFACTOR =0.001.