This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7B67-Q1: Voltage tolerance on OUTPUT Pin

Part Number: TPS7B67-Q1
Other Parts Discussed in Thread: TPS7B4253-Q1, TPS7B7701-Q1

Hi Team,

On customer side, we want to use TPS7B6701-Q1 to replace LT3605. For TPS7B6701-Q1, the voltage tolerance on Output pin is -0.3V~22V. 

But for LT3605, the voltage tolerance on output voltage is -40V~40V.

This parameter is very important for customer, the output voltage may connect to battery for some failure mode in customer's application.

Could you check it and recommend a suitable device for me? Thanks.

 


TPS7B67XX-Q1 datasheet screenshot


lt3605 datasheet screenshot

 

 

BR

Songzhen Guo