Other Parts Discussed in Thread: BQ40Z50
Hello,experts of TI,
There is a urgent issue need to solve.
Battery using a bq4050 gague .
- During the test in normal temperature(25℃),there is a 5% skip of the battery capacity;
- During the test in low temperature(-20℃),there is a 85 % skip of the battery capacity;
- During the test in high temperature(55℃),there is a 7% skip of the battery capacity;
So,I wanna know that how to fix the battery discharge curve so that battery capacity has a acceptable performance among normal/low/high temperature.
THANKS.