Other Parts Discussed in Thread: CSD97396Q4M
HI,
I'd like to know if TPS53659 and power stage CSD97396Q4M should be compatible?
I need to drive P0V9 40A max +/-5% (up to 50/60deg Celcius) on Phase1 by using two CSD97396Q4M
and P1V8 8A max +/-5% (up to 50/60deg Celcius) on Phase1 with one CSD97396Q4M.
Is it possible to get the complete datasheet and the schematic reference for TPS53659?
Thanks
Sebastien