Part Number: BQ24273
Other Parts Discussed in Thread: TMS320F28035, BQ25611D, BQ25150, BQ25616, BQ25618
From my customer:
BQ24273
I have a question about IN voltage range and IN operating range, such as bq24273.
The Max input voltage is 18V but the max operating range is only 10V and the max SW voltage is only 12V. I am confused. Could you tell me what is the different between input voltage range and operating range?
bq24273 questions.pptxCan I use this IC on my Vin 12V and output 3.3V (provide power to system (TMS320F28035 Vin min 2.95V to 3.65V) and charges battery?
See attached snips from the datasheet