I am using the UCC27512 gate driver chip (non-inverting layout) for a flyback converter design and it skips every third gate pulse when sending it control signals at 300kHz. I tried lowering the frequency to 100kHz which fixes the issue. I am using a F28335 Delfino Dev Board Kit to send the gate signals of 3.3V.
Summary:
- UCC27512 Gate Driver Chip
- 5VDD (this is also the power into the board that is supported with caps) [pin 3 VDD]
- 3.3V gate signals at 300kHz from F28335 [pin 1 IN+]
- Gate Resistor ~5ohm [pin 4 OUT]
- Pins 2,5,6 are grounded
- Skips every third pulse
- Works at slower 100kHz