This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM27402 as an led drive board with 12v input and 40 A output(3.6v output)?

Other Parts Discussed in Thread: LM27402, TPS92640, TPS92641

Tool/software: WEBENCH® Design Tools

hello dear,i am looking for an led drive board.my first aim was to use lm3433 but they told me that it is no more availble to use as for LM27402 they recommend it to me for its high power output so the main question is can i use LM27402 as a buck converter as led drive board with 12 v 8 A input and 3.6 v output with output current from 10 or less A till 40 A controlled by pwm.

waiting for your response

best regards