hi
i have a requirement that Vin 5V, Vout 3.3V, Io 375mA
I have a load which is having 100uF at its input.
this Buck converter output is given to the load.
my Buck converter should have current limiting property to avoid inrush current.
Also it should not have output discharge function. Because input to the load should stay for min 500ms through the 100uF.
i have selected TPS62007.
can i connect 100uF at its output?
if you have any other solution let me know