Hello Team,
does the TPS389018 have problems if the MR pin get 3.3V while Vdd is not yet getting 3.3V?
In particular Vdd and MR voltages, come from two different power supplies.
MR gets for short time 3.3V at low impedance (without a pull up resistor), while Vdd is not yet there.
By measuring the MR current it looks that only 10uA flows at 3.5V, thus it looks ok.
Nevertheless the TPS389018 ESD structure is not clear and is not sure if 10uA will always be that and not higher.
Currently a redesign would be needed if a resistor or diode will be added in serie with MR to avoid the problem.
- can you confirm that 3.3V on MR, without Vdd is not a problem?
- If a resistor to limit the current is required, to which value must be that current be limited?
Thanks for the follow up,
SunSet