In a system that's powered from USB, the TPS62203 is creating 3.3 volts, which powers a CPU, that then seeks and gets permission to draw up to 500mA. But prior to that time, we're only allowed to draw 100mA. What inductor and output capacitor values will guarantee that 3.3-volts is reached during the 60mA soft-start time? How long is the 60mA time?