This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS561208EVM-896: High current consumption without connected load

Part Number: TPS561208EVM-896
Other Parts Discussed in Thread: TPS562201EVM-715, TPS562201, TPS561208, TPS561201

Hello,

I measure the current consumption of the TPS56108EVM-896 without load (converter is active, 12V Input, 3,3V Output) and the current consumption is 20.8mA. Is that correct?

The current consumption of the TPS562201EVM-715 is only 0.45mA.