This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2085-V1P3: Flashing Default senc file to BQ2085

Part Number: BQ2085-V1P3
Other Parts Discussed in Thread: BQ2083, BQ2085, BQEVSW, BQ20Z90, BQ20Z65

Hallo experts,

How can I flash the default senc file mentioned in this thread? ->

Should I use the bq2083 EVSW ?

Thanks for helping us.

  • Have you tried with the bq2085 EVSW?

    There is no need to program the whole senc file. Just a .dfi or .rom file is sufficient. Is there a specific reason to program the whole senc file?

  • Hi Shirish,

    thanks for your answer.

    How can I generate a *.dfi or a *.rom. I know these files only from bq20z95 or 20z65 with
    the the bq Evaluation Software (http://www.ti.com/tool/BQ20Z65-R1_BQEVSW-SW).
    For the bq2085 I have to use the bqEVSW, isn´t it? Where can I read back a *.dfi?

    Is there a other EVSW for the bq2085?

    The reason why I do this is because I want to understand the bq2085 better. We have some old products that may need a cell change.

    Thanks for helping us.

  • Hi Shirish,

    thanks for your answer.

    I am using the bq2083 Evaluation Software Version 2.5.0

    How can I generate with this Software a *.dfi or *.rom?
    I know these files only from the bq20z90 or bq20z65 with the bqEvaluation Software ().

    Thanks for helping us.

  • Hi Shirish,

    do you have any news for me?

    Is ist possible to generate a *.dfi or a *.rom with the bq2083 Evaluation Software Version 2.5.0?

    Thanks.

    Klaus

  • Hello Klaus,

    I think there is a flashstream app note on ti.com you can use for this part to convert senc to dfi or rom.

  • Hi Klaus,

    The bq2083 evaluation software does not support *.dfi or *.rom

    It may also not support *.senc, but i am not sure.

  • srec/senc files are normally used to program memory. The bq2085 srec/senc file is not referenced in any document or guide that TI provided for the bq2085. The other thread where the senc was posted for bq2085 was probably for a specific use case, is of unknown origin, and we discourage its use.

    The bq2085 comes preprogrammed with default data. Refer page 38 and 39 of the Datasheet (Memory map section)for information related to the programmable memory.  The Data Flash screen of the evaluation software has all the functions to modify this memory.