Other Parts Discussed in Thread: UCD9248,
I use UCD9248 as power controller and PTD08A020W as power stage. One PTD08A020W module is not enough to supply current considering my application. I use 2 PTD08A020W modules in parallel connection source up to 40A current. I am not sure how to connect the modules in parallel. Can I just connect the VOUT of the two stage? The datasheet shows connecting VOUT is OK. But I am worried if two stages output voltage with a slight difference, the power stage outputing a higher voltage will source the power stage outputing a lower stage.