Hi team,
I have some questions for LM5050-2.
Q1. Would you tell me the behavior of LM5050-2 under operation voltage < 6V ?
We are going to use LM5050-2 to prevend the reverse current between parallel-connected power supplies(12V).
I anxious the reverse current occurs under operation voltage because of the difference of slew rate when power supplies ON or OFF .
Does it needs for external circuit to prevend reverse current under 6V ?
(For example, the voltage monitor circuit of IN pin.)
Q2. If possible, could you provide an LM5050-2 application example of parallel-connected power supplies.?
Q3. Could I use OFF pin under operation voltage 6V to pull down GATE pin ?
Thanks
Best regards,
Akita