This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62800: Output Voltage

Part Number: TPS62800

Hi team,

My customer is looking for an ultra low Iq DC/DC. 

The customer would like to change the two output voltage on the fly(dynamically). Is the TPS62800 able to change the output voltage dynamically to another output voltage by changing the VSEL resistor? If it's not allowed, could you tell me the recommended device?

Vin : Li-Ion 1cell

Vout : 0.5V/0.65V

Iout : TBD, but it should be less than 1A.

Package : Small size like CSP

Regards,

Yamaguchi