Part Number: LM337-N
Other Parts Discussed in Thread: LM337, LM317
hello,
I work with this component in its normal configuration (Figure 1), and according to the resistor ratio, I should be at the output -49Volt.
when I work with the regulator stand-alone it works fine(figure 1)- I measure with DMM -49.1oltage at the output of the regulator.
figure 1:
As soon as I connected resistor and diode between to voltage (-54V, -49V) at another place in the PCB the voltage output regulator drop to ~-52V(Figure 2).
Do you have an idea why? I simulated this circuit and this situation doesn't happen. (do you have another spice model for LM337 besides the one that appears on the site)
figure 2:
regards,
Almog