Other Parts Discussed in Thread: UCC28704
Hi Team,
We are working with the UCC28704 EVM and are adapting it for a non isolated solution, operating off of line voltage input. We connected the secondary negative/ground to the neutral on the EVM with a short (~ 2”). This led to increased conducted emissions in frequency range of about 500KHz to 30MHz (by more than 10 dB). What is causing the emissions? Do you have suggestions for board level changes to the EVM that can reduce the emissions? The layout of the EVM is designed for an isolated solution, but I suspect that if this was redone with non-isolated application in mind we would see improvement. Let me know if you have any suggestions for implementing this.
Regards,
Garret