Other Parts Discussed in Thread: TPS62743, , TPS62840
Hi!
Currently, I'm using TPS62743 to convert 5 V to 1.8 V to power a BME680 which has a peak current of 12 mA during the measurement. Because I can only draw 5 mA at maximum from Vin I'm looking for a more efficient buck converter and found TPS62840 which has lower Iq thant the TPS62743. Later on, I found TPS62808 which has the highest efficiency but a higher Iq. Since Vin is not a battery, I do not care much about Iq except on no load in PWM. Am I right that neither of the bucks will enter PWM at my load conditions?
Would you recommend TPS62808 for my design or should I stay with TPS62743?
BTW: I'm using 47µF for Cout and 220 µF for Cin to reduce ripple and have a large buffer for the measurement which can take up to 120 ms. Sometimes, I encounter startup problems. I believe because of the in-rush current caused by the two capacitors. Would you recommand placing and additional inductor in line before Cin?
--
Many thanks,
Mathias