Other Parts Discussed in Thread: TINA-TI
Hi,
I used Spice-Model: UCCx813-0 and UCCx800 (Date: 06/21/10;Model Version: Final 1.10) and I always get an error message:
u1:vr2: Missing value, assumed 0V @ DC
The simulation is wrong and the voltage on pin vcc = 0V (Stimuli: 8V DC-Source). What is wrong, the parameter vr2 is a internal value from Spice-Model?