This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28810: Can UCC28810 be used for 400V(about100pcs of LED) with 150mA? 1

Part Number: UCC28810
Other Parts Discussed in Thread: UCC28056

 Hello guys,

 One of my customers is considering using UCC28810 or 11 for their next products.

 Their design requirements are the follows.

 Vin: 85V~264V

 Vout: 400V (to drive about 100 pcs of LED)

 ILED: 150mA

 Can UCC28810 or 11be used to drive about100pcs of LED with 150mA?   Or Do you have any reference design for such application?

 Could you please give me your reply?

 Best regards,

 Kazuya.