I have got Troubles with the VCCX pin, pin 6 of LM5140-Q1. When I leave this pin Floating, the converter works. So far so good. In the datasheet it is written on page 3:
"6 VCCX I Optional input for an external bias supply. If VCCX > 4.5 V, VCCX is internally connected to VCC and the internal VCC regulator is disabled. If VCCX is unused, it must be grounded."
So if I do not want to use VCCX (an external 5V supply), then I have to connect the VCCX pin to Ground. I did so. After this Change, the converter did not switch anymore. After removing pin 6 (VCCX) from GND, it did work again.
Is this a flaw in the datasheet or am I doing something wrong? Help is greatly appreciated. Many thanks in advance.
Patrick