This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ21061EVM: Which are the registers need to be set for the charging process

Part Number: BQ21061EVM

Hello,

Which are the registers need to be set for the charging process?

So I have set:

VBAT_CTRL to 4.2V -> 3C

ICHG_CTRL to 500mA ->3C, also tried with lower 150mA

PCHG_CTRL to 50mA-> 94

TERMCTRL to 20% ->28

ILIMCTRL to 600mA -> 07

Charge current step is set 2.5 mA

Disabled TS register CHARGECTRL0

TS control mode(HOT/COLD only)

All other registers I have set to default state.

Battery is samsung 2850mAh(inr18650-29e)

The following is happening:

STAT0 register changes every 10 seconds the bit  CHRG_CV_STAT set active than in 10 seconds  CHARGE_DONE_STAT is set to active. If I put out the battery from the charger and measure the voltage its always 3.6 V.

And can I charge over 500mA with this device?

Thanks