Hi
I have a question regarding the allowed voltage level for the Ven in the LDO.
From the data sheet:http://www.ti.com/lit/ds/symlink/tps7a85.pdf?&ts=1589468396224
Table 6.3 Recommended operating condition state the level is up to Vin voltage level.
The absolute maximum rating the level of Ven is up to 7.0V, the electrical characteristic table define Vin_high of the Enable is up yo 6.5V.
Is there an impact on the MTBF if I operate the LDO with Venable voltage above Vin of the LDO?
I plan to provide 3.3V for the Enable pin voltage level while some of my LDO's the Vin is 1.2V.
According to my understanding, I can do it (I am not in the recommended operating condition), but I would like to understand the impact on the MTBF or other damage that may occur.
Regards
Omer