This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5109B: WSON Coplanarity Data

Part Number: LM5109B


Customer is asking for coplanarity data for the LM5109BSD/NOPB device.

This is WSON(NGT) and I found this E2E post which discusses a 16-pin WSON device.

I quote:

It turns out that the values you see (0.05mm maximum standoff and 0.08mm coplanarity) are specified per JEDEC standards for all WQFN/SON packages. TI follows these standards, and thus these tolerances are included with the package for the DS15BA101.

As such, the DS15BA101 NGQ package will have the same specifications.

As such, is it same to assume that for any WSON package, no matter the pin size, that we meet JEDEC standards and thus have under the maximum coplanarity of 0.08mm?

At the very least, is this LM5109B (WSON) device within JEDEC specs of maximum 0.08mm?

Thanks & Regards,

Darren