This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5018: Channel to channel error

Part Number: LP5018

Hello,

I'm slightly confused on the channel to channel current error spec. The datasheet describes it as +/-7%, but based on the provided equation it seems like the difference between out1 and out2 could be 14%:

If I have Iave set to 10mA, then one channel could be at 9.3mA and the other could be at 10.7ma, making the difference 14% between the two. Is my understanding correct?

Thanks,

Michael