This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PTN04050C: EMI Compliance

Part Number: PTN04050C
Other Parts Discussed in Thread: TPS61089, TPS61088

Hello!
I'm working in a new project for my company and I would like to use the PTN04050C.

But this project must meet the following standards:

CISPR11: Radiated Emission
CISPR11: Conducted Emission
IEC 61000-4-3: Radiated radiofrequency
IEC 61000-4-6: Conducted radiofrequency
IEC 61000-4-8: Magnetic Fields

There is some test reports or other informations that allows me to analyze if this board
can meet theese standars?

Greetings,
Geraldo Gomes.