Other Parts Discussed in Thread: UCC28704
I have a design based on the example in the datasheet, but regulated for 5v output, however I cannot get it to start as the circuit during the exploratory three pulses goes into overvoltage on the output.
I have reviewed the design process and cannot find any glaring issues, however I did find a weird signal on the CS pin.
Channel 1 is the DRV output to the MOSFET and channel 2 is measured on the top of R_CS.
After the exploartory pulses the SD pin signals output overvoltage (as found in another post) and this is very well in line with the output being built up to > 6 v at this time.