Other Parts Discussed in Thread: LM73605-Q1
The datasheet for this part indicates that if an external SYNC signal is being used but is frozen at logic high or logic low meaning no transitions occur, that after a "time-out" the part will revert back to its internal oscillator for SYNC. This is great and a very desirable behavior but I would like to know approximately how long this time-out period is so that I can assess whether I need to provide additional filtering or other protection to handle a brief loss of regulation that might occur during the switch-over. Also, when an external sync is provided I'm assuming that that hand-over happens instantaneously without a corresponding time-out to switch between internal and external sync?