Other Parts Discussed in Thread: TPS2111,
Hi all,
I'm testing a new design and I'm facing the following problem: I set up the TPS2111 in order to have priority on IN1 when both input sources are plugged in (IN1 = 5V from SEPIC power supply, IN2 = 5V from USB, D0 connected to ground and D1 connected to IN1).
When IN1 is connected it's all ok, but when I connect ONLY IN2 (SEPIC input unplugged), after a while, the power mux gets crazy and starts to switch beetween IN1 e IN2 continuously. To prove that, I can see at the input of IN1 1.8/1.9V even if nothing is connected, which would trigger the mux to switch input. I wonder if it is possible that TPS could apply that 1.8/1.9V from the IN1 pin.
Attached you can se the schematic:
Anyone has faced the same problem or could help me, please?
Thank you in advance.