Other Parts Discussed in Thread: LP3992,
Hi Team,
- The circuit system block diagram is as follows. The output waveform of TLV703 produces periodic 2.64V output peak voltage with an interval of 204.5ms. However, when we use LP3992 of Low-Power semi, this problem does not appear. The LDO output waveform and the schematic is shown below:
- The enlarged peak voltage is shown below:
- After checking the input voltage waveform of LDO, it is found that there is no big burr and noise, and the waveform is shown as follows.
- After that, I grabbed the waveform of WiFi SOC, and found that there would be periodic load current changes. The current change is about 150mA, and the reversed current waveform is shown as follows.
- So now I preliminarily locate that the peak voltage is caused by too slow transient response, and prepare to connect another 4.7uf capacitor in parallel at the output terminal.
- Are my analysis and improvement measures correct?
- Are there any better suggestions for improvement?
- What do you think is the source of the peak voltage?
Best regards
Zhihong Huangs