Other Parts Discussed in Thread: GPCCHEM, BQSTUDIO, BQ27421EVM-G1A
Hi TI E2E forum,
I am using the BQ27421 Fuel gauge, and I have noticed that there is a SOC "jump" from the SOC before turning my device off to after turning it back on. The biggest jumps is from a SOC of 70% -> 2%. The SOC stays at 2% whilst the battery is being heavily charged (C/2), or lightly discharged (C/20).
I am not controlling the battery current when the device is turned on, so it may be charging or discharging.
Also worth noting is that I haven’t seen the SOC jumps from a full charge battery at rest (SOC = 100%) going into discharge. I think this is because the SOC cannot be any higher that 100% during the FG initialisation (or OCV measurement). Likewise I didn’t observe SOC jumps from a fully discharged battery (SOC= 0%) going into a charging state, we think that this is because the SOC cannot go lower than 0% during the initialisation going into a charging state.
Continuous charge, rest and discharge cycles as described in learning documents are achievable with the Fuel gauge configuration, and the true SOC errors I have observed are less than +/-5%. Note that I haven't observed SOC jumping is observed when performing these ideal cycles.
Can you please advise where I should look to manage the SOC jumps?
Best regards,
William