Other Parts Discussed in Thread: TPSM846C24
Hello,
I need to know the ESDS (HBM Class Level) rating of the PTH05020WAH. I already contacted the TI Customer Center, and they were only able to provide the following message re: older TI parts: ""If Electrostatic Discharge (ESD) classification is not provided in the data sheet, then it is recommended that the device be treated as ESD sensitive and that it be manufactured using an established industry ESD control programs such as ANSI/ESD S20.20."
After asking for more accuracy re: the ESDS threshold level (i.e. Class rating), I was advised to consult with the product specialists handling our E2E Support Channel.
Can TI management provide any more details re: just 'how ESD sensitive' these devices are? That is, should your customers treat them as a Class 2B, Class 1C, Class 0 (HBM)?? I just need to understand the factual ESDS attributes of this device, so I can properly identify how ESD sensitive our company, suppliers and customers should treat the CCA using these TI devices.
Thank you very much!
Jim Sobe
Sr. Components Engr/ Collins Aerospace