Dear expert,
My customer is using LM5036 in telecom power module.
Vin: 36-75V
Vout:12V
Pout:200W
However customer found that output ripple voltage is large and has low frequency component. Please see sheet 1(Vin=36&48V, Io=16A), the lower the Vin is, the low frequency ripple is larger.
Besides, customer tested on EVM( LM5036EVM-294 without any change), please see sheet 2(Vin=36&48V, Io=8A) still find the low frequency component. Could you help to check on your EVM board?
If this low-frequency ripple cannot be effectively suppressed or eliminated, they'd like to know whether there is a corresponding explanation from TI to explain the cause of the problem. So that they can give a reasonable explanation to the end customer. The main concern of the end customer is that their loop compensation is unstable and there is interference on the layout. Thanks for your support.