Other Parts Discussed in Thread: TPS62147, , TPS62130
I need to know more information about the VOS pin.
Section 10.3.2 from the datasheet says:
In applications where TPS62147, TPS62148 are used to power multiple load circuits, it may be the case that the total capacitance on the output is very large. In order to properly regulate the output voltage, there needs to be an appropriate AC signal level on the VOS pin.
Figure 87 gives an example, but I can't find anywhere in the datasheet information regarding the recommended voltage ripple for a given capacitive load (multiple loads connected to output)
1. How do you decide on the appropriate voltage ripple for a given capacitive load?
2. What happens if the "AC signal" (voltage ripple) is larger/smaller than the required ripple?
Thanks!
Regards