Hi Team,
I would like to find the solution which meet below requirement . I find TPS62808 in ti.com. Do we have more appropriate solution? or next gen roadmap could send me directly?
Description |
Vin |
Vout |
Iout |
Efficiency @1mA |
Iq (typ.) |
Isd (typ.) |
Dimension |
1.8V Buck |
3-4.5V |
1.8V |
>50mA |
>85% |
<5uA |
<300nA |
<1.5mm^2 |
Regards,
Roy