Part Number: TPS25942L
Other Parts Discussed in Thread: TPS2595, TPS24740
Hi Team,
Can the TPS25942L reverse protection be controlled to shut down?
Thanks and best regards,
Jamie
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jamie,
Can you please elaborate your question ?
Do you mean will TPS25942L will shutdown for reverse current protection ?
Hi Praveen,
Sorry for the confusing expression.
I mean is it possible to enable and disable reverse protection?
Thanks and best regards,
Jamie
Hi Jamie,
Unfortunately, we cannot disable the reverse current protection of TPS25942L.
In case you need an efuse with out reverse current protection, you can consider using TPS2595. If you can explain in detail your system use case, I will be able to help you in suggesting a more suitable solution.
Hi Jamie,
Can you explain your system use case so that I will be able to help you better.
Hi Praveen,
Because I saw Reverse protection threshold at -3mV, -9.3mV, -15mV.
Currently BBU design discharge Max. current = 0.2A, If Rds on=42mOHM; V_reverse_i =-0.2*42m= -8.4mV.
It is bound to trigger reverse current protection.
Thanks and best regard,
Jamie
Hi Jamie,
Yes, In case 0.2A reverse current flows in the device, the device can cut off Input and Output.
Hi Jamie,
Hope your question is answered. In case you do not have any further questions, can we close this thread ?