Other Parts Discussed in Thread: LM3880
I am using two of the TPS82084's to power two different rails on a part. The rails are 1.8V and 0.9V. I have a requirement where I need to power up the 0.9V first and then the 1.8V. However on power down it is the opposite of 1.8V first and then 0.9V. How do I use the output discharge feature of the TPS82084 to have the 1.8V rail discharge before the 0.9V? The 0.9V rail is drawing an average of 1A of current the and 1.8V is drawing and average of 26mA. Thanks.