Other Parts Discussed in Thread: BOOSTXL-BATPAKMKII, BQ25616
Hi
I just gotten a BOOSTXL-BATPAKMKII eval board and have a question on charging in standalone mode.
The default Riset (R4) and Rilim (R1) are configured at 500ohm and 270ohm respectively.
I am trying to get the eval board to fast charge at 2A an dhad changed the resistors to
Riset (R4) = 130 ohm, around 1.92A
Rilim (R1) =135ohm, 2A limit
Power supply = connected a 5V/2A PSU from a workbench PSU TTI model
But when I connect a 3.7V Lipo battery (4000mAH) to it, the current drawn from the workbench PSU is only 500mA.??
Have I missed out something that I have not changed to charge the battery in standalone mode?
Updated 20mins later:
a.) Configure EN1 and EN2 to 1, 0 respectively according to datasheet. EN1 tied to 3v3
PSU start to go above 500mA but strange anomaly noticed, after incrementing from 1.4A to 1.6A, the eval board current consumption suddenly flies all over the place. Once 1.6A hit, the PSU current swings to a random current ranging from 0.2A to 0.9A and jumps randomly, not liking this jump. Any advise for this? Had thought there should be CC then CV stage for BQ24250 charging?