Other Parts Discussed in Thread: BQ25606, BQSTUDIO, , GPCCHEM
Hi,
I am using BQ27441-G1A as the fuel gauge with BQ25606 as charging for charging a Lithium-Ion battery with a capacity of 4400 mAh. I have successfully completed the ChemID finding and learning cycle to create a golden file. Unfortunately after configuring the Fuel gauge with the golden file, it showing a jump in SoC to 100% from below 50% while charging. When I checked for the reason I have found that the jump in the Full charge Capacity is causing this issue. I am attaching the log data from Bqstudio while this jump is happening and the ChemID report. Can you help me to find a solution to fix this? 3386.Second_Data-report.zip4118.fuelguage7_Batset-036_partBoard.csv