This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27212: UCC27212 Layout guidelines are referring to a 8 pin device.

Part Number: UCC27212

Hello,

the chapters 10.2 and 10.2.1 need to be changed. Both chapters are referring to a 8 pin device. the UCC27212 is a 10 pin device (WSON 10 pin).

Thanks, Heiko

  • Hello Heiko,

    Thank you for the interest in the UCC27212. Thank you for pointing out the 8 pin layout example for the UCC27212 driver which is a 10 Pin SON package. Many 100V half bridge gate drivers have multiple packages available and the pin assignments are the same, or similar in some cases with unused pins. The same general recommended layout guidelines would apply for the UCC27212 DPR package.

    Confirm if this addresses your questions or you can post additional questions on this thread.

    Regards,