Other Parts Discussed in Thread: TLV62084, TPS62080
TLV62080(A), TLV62084(A), TLV62082
In any cases, the soft start time is described as 40us.
Due to the large capacity of the output line capacitor and the large load current from startup,
If the target voltage could not be reached within the soft start time,
I think it will shift to normal operation and continue to power on.
Switching operation starts 40us after EN is set,
It is described that it starts with a slope of 10 mV/us.
I hope to know if it does not move out of the set voltage at startup, or continue the soft start behavior until the target voltage is reached.
Any advice will be appreciated.
Jin