Other Parts Discussed in Thread: CSD18537NQ5A, TINA-TI
Hello,
I've created a shematic with the webench.
- Vin=18 - 24 V
- Vout=13,5V
- Iout=12A
After that i tried to use the TINA TI transient model of the LM3150 (Rev. A) to simulate the same circuit in TINA TI.
The T3 CSD17320Q5A is a P-Spice Model and the T1 CSD18537NQ5A is a TINA TI model.
Using the transient analysis i get a convergence problem. In the Info is noted: Component: T1.DBD