Hi Team,
I have some questions that I would like to know about output power as soon as possible.
It is used in Parallel as shown in data sheet Figure37.
1. The output voltage standard is 75% Load. Is the shipping test inspected with 75% Load?
2. At light load, it is Typ.7/Max.15 as specified in LOAD REGULATION 10% TO 100% LOAD.
The maximum output voltage at 5V/100mA is about 5.8V.
There is no minimum value regulation.How to find the minimum value of 5V/100mA?
We have created a graph that considers the maximum/average/minimum of expected output fluctuations. Is the understanding correct?
3. The recommended value of Cin described in the circuit diagram of data sheet Figure37 is 2.2uF capacitor at 12V Input.
If 0.1uF is attached to this Cin, will it affect the output voltage?
I would like to know the problem caused by not using the recommended capacitor.
Best Regards,
Kenji