This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62861: what the difference between startup time in datasheet

Part Number: TPS62861

Hi,

customer want to find a part with small delay between Vin and Vout. Vin=5V, Vout=3.3V, Ioutmax=500mA. EN is connect with Vin through dividers. delay between Vin and Vout should be <500us.

I check TPS62861,

which one is the delay between Vin and Vout, 0.2ms or 1000us?

and when I want to find a buck or LDO with lower delay between Vin and Vout, which feature I should check? thanks.

Best regards,

Yuan