Other Parts Discussed in Thread: TPS23758
Hi, we also have some similar issue of evaluating output voltage.
I need to make it slightly higher than 5V, maybe 5.2-5.5V.
Is there any guides or tool kits for us to reference, thank you.
Tim
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, we also have some similar issue of evaluating output voltage.
I need to make it slightly higher than 5V, maybe 5.2-5.5V.
Is there any guides or tool kits for us to reference, thank you.
Tim
Hi , according to EVM R1=200K R2=36.5K we measured Vout=5.1V Vpp=70mV.(Vin source is POE)
As I changed the FB resistance to R1=200K R2=33K we measured Vout=5.7V Vpp=250mV(Vin source is POE)
How do we overcome the Vpp problem in this case? Can we tune the COMP capacitance and resistance to achieve it?
Thank You
Hello Tim,
I am glad to hear you were able to successfully change the output voltage.
To decrease the output ripple, one thing you can do is increase the output capacitance. The following equation is a guideline. Alternatively you can guess and check in the lab :)
Another suggestion is to use electrolytic caps as well.
If this post answers your question, please indicate so by marking this thread as resolved. Thank you.
Regards,
Michael P.
Applications Engineer
Texas Instruments
Hi Micheal, we already increased Cout to 860UF , but it didn't improve much.
So I am wondering, how to progress the FB accuracy in this kind of architecture.(TPS23758 is a primary side regulation system)
Thank you,
Tim
Hello Tim,
When you mention accuracy, are you talking about ripple or load regulation?
You could also try changing the snubber values across the FET Q1 to lower the peak voltage.
Did you use eletrolytic or ceramic caps? Also, what voltage value did the caps have?
Try using 330uF electrolytic and a 0.1uF ceramic on the output.
If this post answers your question, please indicate so by marking this thread as resolved. Thank you.
Regards,
Michael P.
Applications Engineer
Texas Instruments