Tool/software: Code Composer Studio
Hi there,
We have 6 LED strings (28 LED / string) in our design and we plan to drive them with below circuit:
Here are some specs of these LED strings:
- LM3463 [Slave]
- Current per string = 300mA
- Max.Vf per string = 93.8V
- LM3463 [Master]
- String #1 current = 300mA
- Max.Vf string #1= 89.6V
- String #2 current = 460mA
- Max Vf string #2 = 47.6V
Our concern is that on the LM3463 [Master], we may have MOSFET power dissipation issues.
Can you help and confirm if this may be true, and help advice a workaround if needed ?
Thank you.
Regards