This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZM33606: Connection destination GND of SYNC/MODE pin

Part Number: LMZM33606


Hi ALL,
In the data sheet, the GND connected to the SYNC/MODE pin is described as AGND.
However, it is PGND in the schematic (Figue6) of LMZM33606EVM.

Which is correct, AGND or PGND?
Is there no problem with either?

  • Hi,

    The SYNC/MODE pin can be connected to either AGND or PGND. AGND and PGND are internally connected so they are effectively the same node.

    The reason why it was recommended to connect to AGND is because AGND is less populated with noise from the power signals.

    However for SYNC/MODE feature, I don't think it would be an issue connecting to either AGND or PGND.

    Regards,

    Jimmy