Hi team
My customer using the TPS54328 as the 16V to 4V function, the input is the four-cell Li-battery and the fully-charged battery voltage is about 16.4V, the load is a GPRS module in which the startup current can reach up to 2A and the working current is less than 1A.
The question is that the SW node voltage waveform looks a little strange, but the output 4V rail looks stable. I am not sure if it is an expected SW waveform. Could you please tell me under what circumstances would the SW voltage waveform look like this? I want to check whether the customer's circuit is well-designed. The SW detail please refer to the following photos.